TIDUCL3 February 2017
In automotive lighting, EMI is a problem. Therefore, this TI Design was made so that it can be CISPR 25 compliant. In testing it was found that the design is CISPR 25 Radiated Emissions Class 4 compliant as shown in Figure 26, Figure 27, and Figure 28, and is CISPR 25 Conducted Emissions Class 5 compliant as shown in Figure 29.