Make sure the hardware is setup as outlined in Figure 3-30. Do not supply any high voltage (HV) power to the board yet.
powerSUITE Settings : On the powerSUITE page select under Project Options section:
Select Lab 7 under Lab option.
Select input to be DC under PFC INPUT/INV Output options
Also disable the other options such as Non Linear Voltage Loop, Adaptive Deadtime and Phase shedding
Assuming all other options are same as specified earlier in Section 3.1.2.5.5.1.
Under Control Loop Design, options for the current loop tuning automatically be selected (Tuning → Current Loop → COMP1 → DCL_PI_C1). Now click on the Compensation Designer icon ().