3.1.2.5.6.2 Building and Loading Project and Setting up Debug
Right click on the project name,
and click Rebuild Project. The project builds successfully. Click
Run → Debug, which launches a debugging session. In the case
of dual CPU devices, a window may appear to select the CPU the debug must be
performed. In this case, select CPU1. The project then loads on the device, and
CCS debug view becomes active. The code halts at the start of the main
routine.
To add the variables in the watch
and expressions window click View → Scripting Console to open the
scripting console dialog box. On the upper right corner of this console, click
on Open to browse to the setupdebugenv_lab6.js script file, which
is located inside the project folder. This file populates the watch window with
appropriate variables required to debug the system. Click on Continuous
Refresh button () on the watch window to enable continuous update of
values from the controller. The watch window appears as 3.
Figure 3-33 Lab 6 Expressions View
Enable real-time mode by hovering
the mouse on the buttons on the horizontal toolbar, and clicking the
button.