Note: Only one device, the LAUNCHXL-CC2640R2 or XDS110, can be connected to the PC while running the executable file.
- Insert one CR3032 battery into the BT1 connector on the TIDA-01580 board and power it on by using the S2 switch (ensure J8 is shorted on the TIDA-01580 board). Ignore this step if it was already done during programming of the TIDA-01580 board.
- Revert back to the original LaunchPAD jumper settings.
- Plug in the LAUNCHXL-CC2640R2 device on the USB port of the PC.
- Open the Setup_TIDA-01580.exe file and go through the installation process, explained as follows.
- Setup Welcome Screen – click Next.
- License Agreement Screen – Accept the agreement and click Next.
- Installation Directory Screen – click Next.
- Select Components Screen – click Next.
- Ready to Install Screen – click Next.
The setup starts installing and the progress screen is displayed (see Figure 3-16).
- When installed, click Finish. Look for the TIDA-01580 Application.exe at the installed location (default location: C:\Program Files (x86)\Texas Instruments\TIDA-01580\TIDA-01580 Application).
While launching the GUI, a splash screen appears, as shown in Figure 3-18.
The Instructions tab provides instructions and safety precautions for the user, as shown in Figure 3-19.
The Configurations tab (see Figure 3-20) provides information about the software paths.
- Ensure the CCS base-folder path is set to <CCS installation path>\ccsv7\ccs_base.
- Ensure the project .OUT file path is set to <installation folder>\TIDA-01580_firmware\TIDA-01580_firmware_rx\FlashROM_StackLibrary\TIDA-01580_firmware_rx.out.
- The START/STOP button can connect and program the LAUNCHXL-CC2640R2 device to capture the data. After clicking the START/STOP button, the TIDA-01580 board must immediately be power cycled using the S2 switch. The START/STOP button can also disconnect the link.
The HRM tab (see Figure 3-21) shows PPG data taken from green LED and ECG data. The HRM tab estimates heart-rate from both sets of data (time difference in seconds between two peaks of PPG or ECG data / 60).
Note: As soon as the BLE connection is established, the Configurations tab switches to the HRM tab.
The SpO2 tab (see Figure 3-22) shows PPG data taken from the red and IR LEDs. The SpO2 tab estimates % SpO2 from both sets of data.
- The LED indication of BLE Connected? turns on if the LAUNCHXL-CC2640R2 receiver is connected with the TIDA-01580 board over BLE.
- The LED indication of Low Battery turns on if the battery voltage is less than 2 V.
- The LED indication of Lead Off Detect turns on if any one of the ECG electrodes are not connected to the human body.
- The Exit button can disconnect and quit the .exe file.