TIDUDO6B May 2019 – October 2020
Now, the reflected current on the input side of the TPS61099 device is given in Equation 12.
Where, efficiency is taken to be 85% (max 88% at low load of 10 µA), see Equation 13.
Where efficiency is taken to be 50%. Therefore, the net total current from all the branch is given in Equation 14.
Therefore, the calculated battery life of the coin cell is given in Equation 15.
For CR3032, rating = 500 mAh
The measured currents on the TIDA-01580 device are much less than these calculated values, because the calculations are for worst-case performance. The measured values include the following:
Inet = 4.09 mA at Vin = 3 V
Inet = 6.05 mA at Vin = 1.8 V
So Iavg = 5.06 mA, which gives battery life of 98.7 hours.