TIDUDW4B January 2019 – December 2024 CC2640R2F , TMP117
The layout for the flex PCB patch was done on a two-layer board, with the intention of maximizing overall board flexibility. Higher numbers of layers likely limit the bending radius of the board and affects wearer comfort. For general recommendations for flex PCBs, consult with the desired manufacturer of the flex board. These boards are extremely thin, therefore the boards can be sensitive to heat applied during the process of soldering or reflow. It is important that this aspect be considered to minimize potential damage to the board traces. If reliability is a concern, consider applying a semi-rigid design form factor by applying a stiffener to portions of the board not intended to bend.