TIDUE59A May 2018 – September 2020
Currently, support for editing and building the source is limited to Code Composer Studio™ (CCS) only, but the project could be moved to other IDEs and compilers, such as IAR or GCC. To use the example, download the following:
When the tools and SDK are installed, run the installer for the TIDC-01005 software. The installer will attempt to place the software in the CC3220 SDK by default. If the default path used by the installer does not match the actual location of the CC3220 SDK on the PC, it must be updated. Once installed, the zip file containing the software package must be extracted into the CC3220 SDK under the RTOS demos folder for the CC3220S (extracted contents should end up under <SDK Install Location>/simplelink_cc32xx_sdk_2_10_00_04/examples/rtos/CC3220S_LAUNCHXL/demos). The installed package includes the software source files along with a UniFlash project (.zip file), which provides two different options for evaluating the system.