TIDUE59A May 2018 – September 2020
To accurately measure the power consumption of the DRV8837 on the DRV8837EVM, several hardware modifications are required, in addition to the modifications described in Section 3.1.1. The complete list of hardware modifications required to accurately measure the power consumption of the DRV8837 follows (see Figure 3-13):
When the modifications are complete, the following connections must be made to the DRV8837EVM to perform the power measurement (see Figure 3-14).
When testing the TIDC-01005, a 5-V input was used to power the DRV8837.