TIDUEA0A March 2019 – September 2020
The TIDA-010002 board was initially tested for proper operation using the USB2ANY Interface Adapter, which features I2C-bus protocol support. Both read and write slave access to the TMP117 was verified after correct wiring of the VDD, GND, SDA, and SCL lines between the TIDA-0100012 design and USB2ANY tool.
The fully assembled probes with TIDA-010002 inside, as shown in Figure 3-1, were used for testing. These digital temperature probes (see the 4-wire white cable with 6 m length as an example) were produced by JUMO GmbH & Co. KG in Germany. JUMO is a market leader in the development of industrial temperature probes for a variety of applications, including residential and commercial heat meters. JUMO can be contacted with inquiries about digital temperature probes based upon TIDA-010002 at HeatMeter@jumo.net.
Next, the full TIDA-010002 based digital probe was attached to the MSP430FR6047 Ultrasonic Sensing Evaluation Module using the BoosterPack™ Plug-in Module extension connectors J5 and J6. Table 3-1 shows the four connections required, where the VDD for the digital temperature sensor can be provided continuously or by a GPIO pin for easy power-on and off.
MSP430FR6047EVM | TIDA-010002 | COMMENT |
---|---|---|
SCL (J5.17) | SCL | I2C from eUSCI_B0 |
SDA (J5.19) | SDA | I2C from eUSCI_B0 |
GND (J6.2) | GND | |
GPIO P8.0 (J6.18) | VDD on/off | used for power cycling of the first DRTD |
GPIO P7.5 (J6.20) | VDD on/off | used for power cycling of the second DRTD |
VDD (J5.1) | VDD | alternative to GPIO8.0; used for continuous powering of DRTD |