TIDUEU6B September 2020 – December 2021 OPA810
When the unknown impedance is capacitive as shown in Figure 2-3, the feedback transfer function can be calculated using Equation 2.
The transfer function implies that a zero is formed in 1/β. The frequency of this zero can be calculated using Equation 3.
It can be seen that the zero frequency depends on the unknown capacitance, CX. In Figure 2-4 it can be seen that Aolβ has a rate of closure of 40dB/dec. When the zero frequency is more than a decade below fCL, the phase margin will reduce to zero making the circuit unstable.