TIDUF76 June 2024
This reference design is based on the mmWave demo (mmwave_demo) processing chain from the mmWave low-power software development kit (MMWAVE-L-SDK). The reference design demo uses a BPM-MIMO scheme and contains additional features such as radar cube compression, maximum velocity extension, dynamic clutter removal, and a group tracker.
PARAMETER | SPECIFICATIONS | DETAILS |
---|---|---|
Maximum range (m) | 120 | This is the maximum range supported by the chirp configuration shown in Table 2-1. The maximum detectable range for a given object depends on the Radar cross section (RCS) of the object |
Range resolution (m) | 0.94 | This is the minimum range difference over which two individual point targets can be distinguished by the chirp configuration shown in Table 2-1. The theoretical achievable resolution by AWRL1432 is 3.75cm based on 4GHz bandwidth. |
Maximum velocity (kmph) | ±144 | This is the extended maximum velocity obtained using the Chinese Remainder Theorem on alternating frames. |
Velocity resolution (kmph) | 1.13 | This parameter represents the capability of the radar sensor to distinguish between two or more objects at the same range but moving with different velocities. |
Azimuth angular resolution (Deg) | 20 | This is the native azimuth angular resolution based on the virtual array aperture |