To start CCS and open the project, complete the following steps:
- Connect an isolated AC power source capable of
providing universal input up to 300 W to the input
terminals (connector J5) of the reference board as
shown in Figure 3-23. Set the power supply current limit to 2A. Do
not turn the power supply on at this time.
- Connect a motor to J10.
- Follow Steps 2 and 3 of Section 3.3.4.1.1 to open the project.