TIDUF77 June 2024 MSPM0G1507
Run the GUI software on the host PC. Wait for GUI window to pop up. Figure 3-5 shows the steps to connect the host PC to this reference design board via UART. The default baud rate is 384600bps. The user must change the baud rate setting on both GUI and C2000 if the user wants to use the different UART speed.
A successful connection and communication can be verified by the number of Transmitted Data and Received Data. Figure 3-6 shows that both numbers increase continuously with a successful connection. Those transmitted and received data can be viewed by checking View Tx Text and View Rx Text; however, do not check these features to view when the motor is running.