3.4.6.2 Building and Loading the Project and Setting up Debug Environment
Right-click on the project name
and click Rebuild Project. The project builds successfully. In the
Project Explorer, make sure the correct target configuration file is set as
Active under targetConfigs.
Then, click Run →
Debug to launch a debugging session. The project then loads
on the device and the CCS debug view becomes active. The code halts at the start
of the main routine.
To add the variables in the
watch/expressions window, click View → Scripting Console to
open the scripting console dialog box. On the upper right corner of this
console, click on open and then browse to the
setupdebugenv_chAll.js script file located inside the
project folder. This populates the watch window with the appropriate variables
needed to debug the system.
Click on the Continuous
Refresh button on
the watch window to enable continuous update of values from the controller.