3.2.2.4.3.1 Building and Loading the Project and Setting Up Debug
Open the vienna_settings.h file, set VIENNA_INCR_BUILD to
3.
Right click on the project name, and click Rebuild Project. The project builds
successfully. Click Run → Debug, which launches a debugging
session. In the case of dual CPU devices, if a window appears indicating a CPU
must be selected, then perform a debug. In this case, select CPU1. The project
then loads on the device, and CCS debug view becomes active. The code halts at
the start of the main routine.
To add the variables in the Watch or Expressions window, click
View → Scripting Console to open the scripting console dialog
box. On the upper right corner of this console, click on Open to browse
to the setupdebugenv_build3.js script file located inside the project
folder. This file populates the Watch window with appropriate variables
needed to debug the system. Click on the Continuous Refresh button
() on the
Watch window to enable continuous update of values from the
controller. Figure 3-23 illustrates the Watch window.
Figure 3-23 Build Level 3:
Expressions View
Enable real-time mode by hovering the mouse on the buttons on the horizontal toolbar and clicking the button.