This is the programmer's guide for the DLPC3470 DLP® display and light controller (used with the DLP2010LC DMD) and the DLPC3478 DLP display and light controller (used with the DLP3010LC DMD). This guide primarily discusses the I2C interface of these controllers. For additional information please visit the desired device product folder on ti.com.
DLP® is a registered trademark of Texas Instruments.
Arm® and Cortex® are registered trademarks of Arm Limited.
All trademarks are the property of their respective owners.
This document details the software interface requirements for a DLPC347x DLP® Pico™ Light Controller based system. The DLPC347x DLP Pico Light Controllers support Display, 3D Light Control, and 3D printing applications with the use of several TRP DMD chips. Target markets include:
The DLPC347x has three modes for use in Light Control applications:
External Pattern Streaming mode displays pattern data received via an external video port. Figure 1-1 shows a system configured for this mode.
Internal Pattern Streaming mode displays 1D pattern data stored in flash. Figure 1-2 shows a system configured for this mode.
Splash Pattern mode displays 2D patterns stored as images in flash. Figure 1-2 shows a system configured for this mode.