This application note discusses how to measure total harmonic distortion plus noise or THD + N of an operational amplifier, how to interpret the measurements, and the fundamental principles of THD + N.
All trademarks are the property of their respective owners.
In an ideal amplifier circuit, the operational amplifier or op amp can perfectly output the signal of interest without modification to the phase or waveform shape.
A Fast Fourier Transform or FFT converts a signal into its spectral components and provides frequency information about the signal. Figure 1-2 shows an FFT for a pure 1 kHz sine wave with an amplitude of 1 V peak seen on the ideal amplifier output. The FFT shows only the fundamental frequency and no noise. This is the ideal case. The FFT shows no other frequency components in addition to the 1 kHz fundamental frequency indicating that the amplifier did not distort the input signal.
Real
amplifiers have non-linear characteristics and limitations that distort the input
signal adding harmonics and noise that can be seen in an FFT as shown in Figure 1-3. The FFT is a measurement made at the output of the amplifier that is
configured in a gain of 1 V/V. The y-axis is in units of volts root mean squared
or VRMS. The input signal to the amplifier is a 1 kHz sine wave with a
magnitude of 6 VRMS. The signal harmonics are seen in Figure 1-3 and are integer multiples of the 1 kHz fundamental frequency. Signal harmonics
are highlighted at 2 kHz,
3 kHz, and 4 kHz, however
higher order signal harmonics are also visible up to 10 kHz. The test equipment
and circuit power supply are connected to a 120 VAC (volts alternating current) 60
Hz power outlet. The 60 Hz power line cycle and integer multiples of 60 Hz are
also present in the FFT. In audio circuits, 60 Hz is often described to sound like
a hum when it is coupled into the signal chain.
Total harmonic distortion plus noise is a measurement that provides a figure of merit for a circuits ability to accurately output a signal seen at it's input. THD + N is an important measurement in audio systems. Audio systems with low THD + N provide a more accurate representation of how the audio was intended to sound. Equation 1 mathematically shows that THD + N is defined as the ratio of the harmonic power measurements summed together to the power of the fundamental frequency.
Where:
Vi | RMS voltage of the ith harmonic of the fundamental (i=2,3,4…) |
Vn | RMS noise voltage of the circuit |
Vf | RMS voltage of the fundamental |