SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The TMS320F28P65x is being offered as a Functional Safety Compliant Safety Element out of Context (SEooC) product. This implies that TMS320F28P65x was developed in compliance with TI's ISO-9001/IATF-16949 compliant hardware product development process. Subsequently, this product was independently assessed to meet a systematic capability compliance of ASIL D (according to ISO-26262:2018) and SIL 3 (according to IEC-61508:2010), see Certification for Functional Safety Hardware Process. As such, this safety manual is intended to be informative only to help explain how to use the features of TMS320F28P65x device to assist the system designer in achieving a given ASIL or SIL level. System designers are responsible for evaluating this device in the context of their system and determining the system-level ASIL or SIL coverage achieved therein.
This document is the Functional Safety Manual for the TMS320F28P65x MCU series from Texas Instruments which is part of the high performance C2000™ real-time microcontroller product line. The C2000 product line utilizes a common safety architecture that is implemented for multiple products in automotive and industrial applications.
The products supported by this document have been assessed to be meet a systematic capability compliance of ASIL-D (according to ISO 26262) and SIL-3 (according to IEC 61508). For more information, see Certification for Functional Safety Hardware Process.
This Functional Safety Manual is part of the Functional Safety-Compliant design package to aid customers who are designing systems in compliance with ISO26262 or IEC61508 functional safety standards.
Table 1-1 shows a complete list of the products supported by this safety manual.
Orderable Devices | |
---|---|
Dual-Core Part Numbers | Single-Core Part Numbers |
F28P650DK9NMR | F28P650SK7NMRR |
F28P650DK9NMRR | F28P650SK7PTP |
F28P650DK9PTP | F28P650SK7ZEJR |
F28P650DK9ZEJ | F28P650SK6PZPR |
F28P650DK9ZEJR | F28P650SK6NMRR |
F28P650DK7NMRR | F28P650SK6PTP |
F28P650DK7PTP | F28P650SK6ZEJR |
F28P650DK7ZEJR | F28P659SH6PZPRQ1 |
F28P650DK8NMRR | F28P659SH6PTPQ1 |
F28P650DK8PTP | F28P650SH7NMRR |
F28P650DK8ZEJR | F28P650SH7PTP |
F28P659DK8PZPQ1 | F28P650SH7ZEJR |
F28P659DK8PZPRQ1 | F28P650SH6PZPR |
F28P659DK8PTPQ1 | F28P650SH6NMRR |
F28P659DK8ZEJQ1 | F28P650SH6PTP |
F28P659DK8ZEJRQ1 | F28P650SH6ZEJR |
F28P650DK6PZP | |
F28P650DK6PZPR | |
F28P650DK6NMRR | |
F28P650DK6PTP | |
F28P650DK6ZEJR | |
F28P659DH8PZPRQ1 | |
F28P650DH6PZPR | |
F28P650DH6NMRR | |
F28P650DH6PTP | |
F28P650DH6ZEJR |
This Functional Safety Manual provides information needed by system developers to assist in the creation of a safety critical system using a supported TMS320F28P65x MCU. This document contains:
The following information is documented in the Detailed Safety Analysis Report (SAR) section of the FMEDA, for TMS320F28P65x C2000™ Safety Critical Microcontrollers, which is only available under a Functional Safety NDA and is not repeated in this document:
It is expected that the user of this document should have a general familiarity with the TMS320F28P65x product families. More information can be found at www.ti.com/C2000.
This document is intended to be used in conjunction with the pertinent data sheets, technical reference manuals, and other documentation for the products being supplied.
For information which is beyond the scope of the listed deliverables, please contact your TI sales representative or www.ti.com.