Key Input Parameter | Key Output Signal | Recommended Device |
---|---|---|
SPI or I2C communication to set a programmable threshold, 0-V to 5.5-V analog input | Digital output of a comparator and data captured in NVM | DAC63204, DAC53204, DAC43204, DAC63004, DAC53004, DAC63202, DAC53202, DAC63002, DAC53002 |
Objective: Configure a smart DAC as a programmable comparator with hysteresis or a latching output, programmable window comparator, and save critical registers into NVM when a fault is detected.
This circuit uses a four-channel buffered voltage-output DAC, such as the DAC63204, DAC53204, or DAC43204 (DACx3204), to create a comparator with a programmable threshold value. The DACx3204 has additional comparator features such as hysteresis, a latching output, or a window comparator mode. There is also a fault dump mode available which saves a few registers in the non-volatile memory (NVM) when the FAULT-DUMP bit in the register map is triggered or the general-purpose input/output (GPIO) pin, configured for fault dump mode, is triggered. This feature is useful in system-level fault management to capture the state of the device at the time the fault occurred. In this design, the integrated buffer acts as a comparator and the output of the DAC acts as the threshold for the comparator. The integrated buffer has an exposed feedback path via the feedback pin (FB) which acts as the voltage input to the comparator. All register settings are saved using the integrated non-volatile memory (NVM), enabling the device to be used without runtime software, even after a power cycle or reset. This circuit can be used in applications such as laser distance measurement, cordless vacuum cleaner, or medical accessories.
This schematic is used for the following simulation of the DAC63204. The OUT0 and FB0 signals are measured on an oscilloscope at the test points marked on the schematic.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 1-kHz triangle wave is applied to the input of the comparator (FB0 pin). The threshold value for the comparator is set to 1.25 V in the DAC-0-DATA register. The code programmed to these registers, in decimal, is calculated using:
The following plot shows the comparator output responding to the 1-kHz triangle wave on the FB0 pin. OUT0 changes as the triangle wave goes above or below the 1.25-V threshold set in the DAC-0-DATA register. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 1-kHz triangle wave is applied to the input of the comparator (FB0 pin). The high threshold value for the comparator is set to 3.75 V in the DAC-0-MARGIN-HIGH register, and the low threshold is set to 1.25 V in the DAC-0-MARGIN-LOW register. The codes programmed to these registers, in decimal, are calculated using:
The following plot shows the comparator output responding to the 1-kHz triangle wave on the FB0 pin. OUT0 is high when the input goes above the 1.25-V threshold stored in DAC-0-MARGIN-LOW and is low when the input goes below the 3.75-V threshold stored in DAC-0-MARGIN-HIGH. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 10-Hz triangle wave is applied to the input of the comparator (FB0 pin). The high threshold value for the comparator is set to 3.75 V in the DAC-0-MARGIN-HIGH register, and the low threshold is set to 0 V in the DAC-0-MARGIN-LOW register. The codes programmed to these registers, in decimal, are calculated using:
The following plot shows output responding to the 10-Hz triangle wave on the FB0 pin. The comparator output is reset right before the first rising edge of OUT0. The OUT0 value is latched low after the input is greater than the 3.75-V threshold stored in DAC-0-MARGIN-HIGH. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1. Reset the comparator by writing 1 to the RST-CMP-FLAG-0 bit in the COMMON-DAC-TRIG register.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 10-Hz triangle wave is applied to the input of the comparator (FB0 pin). The high threshold value for the comparator is set to 5 V in the DAC-0-MARGIN-HIGH register, and the low threshold is set to 1.25 V in the DAC-0-MARGIN-LOW register. The codes programmed to these registers, in decimal, are calculated using:
The following plot shows output responding to the 10-Hz triangle wave on the FB0 pin. The comparator output is reset right before the first falling edge of OUT0. The OUT0 value is latched high after the input is less than the 1.25-V threshold stored in DAC-0-MARGIN-LOW. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1. Reset the comparator by writing 1 to the RST-CMP-FLAG-0 bit in the COMMON-DAC-TRIG register.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 1-kHz triangle wave is applied to the input of the comparator (FB0 pin). The high threshold value for the comparator is set to 3.75 V in the DAC-0-MARGIN-HIGH register, and the low threshold is set to 1.25 V in the DAC-0-MARGIN-LOW register. The GPIO pin is configured as an output and is mapped to WIN-CMP-0 by setting the GPO-CONFIG bit in the GPIO-CONFIG register to 0b1000. If using the DAC63204EVM board, remove jumper J6 so the GPIO pin is not connected to the EVM controller. The codes programmed to these registers, in decimal, are calculated using:
The following plot shows output responding to the 1-kHz triangle wave on the FB0 pin. The GPIO value mapped to WIN-CMP-0 is high when the input goes above the 3.75-V threshold stored in DAC-0-MARGIN-HIGH or below the 1.25-V threshold stored in DAC-0-MARGIN-LOW and is low when the input is within the window set by the two thresholds. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1.
The 5-V VDD supply input is used as the reference and a 0-V to 5-V, 1-kHz triangle wave is applied to the input of the comparator (FB0 pin). The high threshold value for the comparator is set to 3.75 V in the DAC-0-MARGIN-HIGH register, and the low threshold is set to 1.25 V in the DAC-0-MARGIN-LOW register. The GPIO pin is configured as an output and is mapped to WIN-CMP-0 output by setting the GPO-CONFIG bit in the GPIO-CONFIG register to 0b1000. If using the DAC63204EVM board, remove jumper J6 so the GPIO pin is not connected to the EVM controller. The codes programmed to these registers, in decimal, are calculated using:
This plot shows output responding to a 0-V to 5-V, 10-Hz triangle wave input on FB0 pin. The comparator output is reset right before the first falling edge of OUT0. The GPIO value mapped to WIN-CMP-0 is latched when the input is greater than the DAC-0-MARGIN-HIGH threshold level. The polarity of OUT0 can be reversed by setting the CMP-0-INV-EN bit to 1. Reset the comparator by writing 1 to the RST-CMP-FLAG-0 bit in the COMMON-DAC-TRIG register.
The 5-V VDD supply input is used as the reference. The input of the comparator (FB0 pin) is set to a step input from 3.75 V to 1.25 V. The threshold value for the comparator is set to 2.5 V in the DAC-0-DATA register. The OUT0 pin is connected to the GPIO pin which is configured as an input and mapped to trigger the fault dump sequence on a falling edge. Make sure the CMP-0-INV-EN bit is configured according to the polarity of the fault signal. If the fault dump needs to be triggered when the input is lower than the threshold, then set the CMP-0-INV-EN bit to 1. If the fault dump needs to be triggered when the input is higher than the threshold, then set the CMP-0-INV-EN bit to 0.
The data captured in the NVM after the fault dump can be read by following this sequence:
NVM ROWS | B31–B24 | B23–B16 | B15–B8 | B7–B0 |
---|---|---|---|---|
Row 1 | CMP-STATUS[7:0] | Don't care | ||
Row 2 | DAC-0-DATA[15:8] | DAC-1-DATA[15:8] | DAC-2-DATA[15:8] | DAC-3-DATA[15:8] |
The following figure shows the terminal window which shows the fault dump storage readback after the GPIO falling edge. The most significant 8 bits of each DAC register are read back in the 2nd row of the fault dump storage. Random DAC values were stored in channels 1–3 for this example. The comparator status bits are shown in the most significant bits of the 1st NVM row. The status for comparator 0 is low. See the full pseudocode sequence in the Fault Dump Pseudocode Example.
The following table shows an example register map for this application. The values given here are for the design choices made in the Programmable Window Comparator with Latching Output Results section.
Register Address | Register Name | Setting | Description |
---|---|---|---|
0x1F | COMMON-CONFIG | 0x8FF9 | [15] 0b1: Write 0b1 to set the window comparator output to a latching output |
[14] 0b0: Device not locked | |||
[13] 0b0: Fault-dump read enable at address 0x00 | |||
[12] 0b1: Disables the internal reference | |||
[11:10] 0b11: Powers-down VOUT3 | |||
[9] 0b0: Powers-down IOUT3 | |||
[8:7] 0b11: Powers-down VOUT2 | |||
[6] 0b0: Powers-down IOUT2 | |||
[5:4] 0b11: Powers-down VOUT1 | |||
[3] 0b0: Powers-down IOUT1 | |||
[2:1] 0b11: Powers-up VOUT0 | |||
[0] 0b0: Powers-down IOUT0 | |||
0x24 | GPIO-CONFIG | 0x3000 | [15] 0b0: Glitch filter disabled for GP input |
[14] 0b0: Don't care | |||
[13] 0b1: Write 0b1 to enable output mode on GPIO pin | |||
[12:9] 0b1000: Selects the WIN-CMP-0 function setting mapped to GPIO as output | |||
[8:5] 0b0000: Disables GPI function on all channels | |||
[4:1] 0b0000: Configures the function of the GPI | |||
[0] 0b0: Disables input mode for GPIO pin | |||
0x20 | COMMON-TRIGGER | 0x0002 | [15:12] 0b0000: Write 0b0101 to unlock the device |
[11:8] 0b0000: Write 0b1010 to trigger a POR reset | |||
[7] 0b0: LDAC not triggered | |||
[6] 0b0: DAC clear not triggered | |||
[5] 0b0: Don't care | |||
[4] 0b0: Fault-dump is not triggered | |||
[3] 0b0: PROTECT function not triggered | |||
[2] 0b0: Fault-dump read not triggered | |||
[1] 0b1: Write 0b1 to store applicable register settings to the NVM | |||
[0] 0b0: NVM reload not triggered. Write 0b1 to reload applicable registers with existing NVM settings | |||
0x03, 0x09, 0x0F, 0x15 | DAC-X-VOUT-CMP-CONFIG | 0x0405 | [15:13] 0b000: Don't care |
[12:10] 0b001: Selects VDD as reference with 1× gain | |||
[9:5] 0x00: Don't care | |||
[4] 0b0: Set OUTx pins as push-pull in comparator mode | |||
[4] 0b0: Set OUTx pins as push-pull in comparator mode | |||
[3] 0b0: Comparator output consumed internally | |||
[2] 0b1: FBx input has finite impedance | |||
[1] 0b0: Comparator output not inverted | |||
[0] 0b1: Enables comparator mode | |||
0x05, 0x0B, 0x11, 0x17 | DAC-X-CMP-MODE-CONFIG | 0x0800 | [15:12] 0x0: Don't care |
[11:10] 0b10: Comparator configured in window comparator mode | |||
[9:0]: 0x000: Don't care | |||
0x01, 0x07, 0x0D, 0x13 | DAC-X-MARGIN-HIGH | 0xC000 | [15:4] 0xC00: 12-bit data updates the MARGIN-HIGH code |
[3:0] 0x0: Don't care | |||
0x02, 0x08, 0x0E, 0x14 | DAC-X-MARGIN-LOW | 0x4000 | [15:4] 0x400: 12-bit data updates the MARGIN-LOW code |
[3:0] 0x0: Don't care | |||
0x21 | COMMON-DAC-TRIG | 0x8000 | [15] 0b1: Resets latching or window comparator on channel 0 |
[14] 0b0: Channel 0 margin low not triggered | |||
[13] 0b0: Channel 0 margin high not triggered | |||
[12] 0b0: Channel 0 function generator not triggered | |||
[11:9] 0x0: Channel 1 triggers not affected | |||
[7:4] 0x0: Channel 2 triggers not affected | |||
[3:0] 0x0: Channel 3 triggers not affected |
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Normal Programmable Comparator Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and enables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x0D
6: //Comparator has no hysteresis or window function
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x00, 0x00
8: //Write threshold to DAC-0-DATA
9: //With 16-bit left alignment 0x400 becomes 0x4000
10: WRITE DAC-0-Data(0x19), 0x40, 0x00
11: //Save settings to NVM
12: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Programmable Comparator With Hysteresis Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and enables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x0D
6: //Configure comparator for hysteresis mode
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x04, 0x00
8: //Write high threshold to DAC-0-MARGIN-HIGH
9: //With 16-bit left alignment 0xC00 becomes 0xC000
10: WRITE DAC-0-MARGIN-HIGH(0x01), 0xC0, 0x00
11: //Write low threshold to DAC-0-MARGIN-LOW
12: //With 16-bit left alignment 0x400 becomes 0x4000
13: WRITE DAC-0-MARGIN-LOW(0x02), 0x40, 0x00
14: //Save settings to NVM
15: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Active Low Latching Comparator Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and enables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x0D
6: //Configure comparator for hysteresis mode
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x04, 0x00
8: //Write high threshold to DAC-0-MARGIN-HIGH
9: //With 16-bit left alignment 0xC00 becomes 0xC000
10: WRITE DAC-0-MARGIN-HIGH(0x01), 0xC0, 0x00
11: //Write low threshold to DAC-0-MARGIN-LOW (set to zero-scale to latch)
12: WRITE DAC-0-MARGIN-LOW(0x02), 0x00, 0x00
13: //Save settings to NVM
14: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
15:
16: //Resets latching comparator output
17: WRITE COMMON-DAC-TRIG(0x21), 0x80, 0x00
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Active High Latching Comparator Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and enables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x0D
6: //Configure comparator for hysteresis mode
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x04, 0x00
8: //Write high threshold to DAC-0-MARGIN-HIGH (set to full-scale to latch)
9: //With 16-bit left alignment 0xFFF becomes 0xFFF0
10: WRITE DAC-0-MARGIN-HIGH(0x01), 0xFF, 0xF0
11: //Write low threshold to DAC-0-MARGIN-LOW
12: //With 16-bit left alignment 0x400 becomes 0x4000
13: WRITE DAC-0-MARGIN-LOW(0x02), 0x40, 0x00
14: //Save settings to NVM
15: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
16:
17: //Resets latching comparator output
18: WRITE COMMON-DAC-TRIG(0x21), 0x80, 0x00
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values provided are for the design choices made in the Programmable Window Comparator Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and disables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x05
6: //Configure comparator for window comparator mode
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x08, 0x00
8: //Write high threshold to DAC-0-MARGIN-HIGH
9: //With 16-bit left alignment 0xC00 becomes 0xC000
10: WRITE DAC-0-MARGIN-HIGH(0x01), 0xC0, 0x00
11: //Write low threshold to DAC-0-MARGIN-LOW
12: //With 16-bit left alignment 0x400 becomes 0x4000
13: WRITE DAC-0-MARGIN-LOW(0x02), 0x40, 0x00
14: //Configure GPIO as output for Channel 0 window comparator
15: WRITE GPIO-CONFIG(0x24), 0x30, 0x00
16: //Save settings to NVM
17: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Programmable Window Comparator with Latching Output Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0, configures latching window comparator
3: WRITE COMMON-CONFIG(0x1F), 0x8F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and disables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x05
6: //Configure comparator for window comparator mode
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x08, 0x00
8: //Write high threshold to DAC-0-MARGIN-HIGH
9: //With 16-bit left alignment 0xC00 becomes 0xC000
10: WRITE DAC-0-MARGIN-HIGH(0x01), 0xC0, 0x00
11: //Write low threshold to DAC-0-MARGIN-LOW
12: //With 16-bit left alignment 0x400 becomes 0x4000
13: WRITE DAC-0-MARGIN-LOW(0x02), 0x40, 0x00
14: //Configure GPIO as output for Channel 0 window comparator
15: WRITE GPIO-CONFIG(0x24), 0x30, 0x00
16: //Save settings to NVM
17: WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
18:
19: //Resets latching comparator output
20: WRITE COMMON-DAC-TRIG(0x21), 0x80, 0x00
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC63204. The values given here are for the design choices made in the Fault Dump Results section.
1: //SYNTAX: WRITE <REGISTER NAME (Hex code)>, <MSB DATA>, <LSB DATA>
2: //Powers up voltage output on channel 0
3: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
4: //Configure Channel 0 with Gain=1x and VDD as reference, enables comparator mode with finite input impedance, and enables comparator output on OUT0
5: WRITE DAC-0-VOUT-CMP-CONFIG(0x03), 0x04, 0x0D
6: //Comparator has no hysteresis or window function
7: WRITE DAC-0-CMP-MODE-CONFIG(0x05), 0x00, 0x00
8: //Write code for 2.5 V threshold to DAC-0-DATA
9: //With 16-bit left alignment 0x800 becomes 0x8000
10: WRITE DAC-0-Data(0x19), 0x80, 0x00
11: //Write random values for other DAC-DATA registers to verify the fault dump readback for this example
12: WRITE DAC-1-Data(0x1A), 0x41, 0x00
13: WRITE DAC-2-Data(0x1B), 0xFA, 0xF0
14: WRITE DAC-3-Data(0x1C), 0x30, 0x00
15: //Configure GPIO as input for fault dump trigger
16: WRITE GPIO-CONFIG(0x24), 0x00, 0x05
17:
18: //Read fault dump storage
19: //Selecting 1st row of fault dump NVM storage
20: WRITE COMMON-CONFIG(0x1F), 0x0F, 0xF9
21 //Copies data from selected NVM to SRAM address 0x9D and 0x9E
22: WRITE COMMON-TRIGGER(0x20), 0x00, 0x04
23: //Write 8-bit SRAM address
24: WRITE SRAM-CONFIG(0x2B), 0x00, 0x9D
25: //Readback least significant 16-bits data from 1st row
26: READ SRAM-DATA (0x2B)
27: //Write 8-bit SRAM address
28: WRITE SRAM-CONFIG(0x2B), 0x00, 0x9E
29: //Readback most significant 16-bits data from 1st row
30: READ SRAM-DATA (0x2B)
31:
32: //Selecting 2nd row of fault dump NVM storage
33: WRITE COMMON-CONFIG(0x1F), 0x2F, 0xF9
34: //Copies data from selected NVM to SRAM address 0x9D and 0x9E
35: WRITE COMMON-TRIGGER(0x20), 0x00, 0x04
36: //Write 8-bit SRAM address
37: WRITE SRAM-CONFIG(0x2B), 0x00, 0x9D
38: //Readback least significant 16-bits data from 2nd row
39: READ SRAM-DATA (0x2B)
40: //Write 8-bit SRAM address
41: WRITE SRAM-CONFIG(0x2B), 0x00, 0x9E
42: //Readback ost significant 16-bits data from 2nd row
43: READ SRAM-DATA (0x2B)
Device | Key Features | Link |
---|---|---|
DAC63204 | 4-channel, 12-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC63204 |
DAC53204 | 4-channel, 10-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC53204 |
DAC43204 | 4-channel, 8-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC43204 |
DAC63004 | 4-channel, ultra-low-power, 12-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC63004 |
DAC53004 | 4-channel, ultra-low-power, 12-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC53004 |
DAC63202 | 2-channel, 12-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC63202 |
DAC53202 | 2-channel, 10-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC53202 |
DAC63002 | 2-channel, ultra-low-power, 12-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC63002 |
DAC53002 | 2-channel, ultra-low-power, 10-bit, VOUT and IOUT smart DAC with I2C, SPI and Hi-Z out during power off | DAC53002 |
Find other possible devices using the Parametric search tool.
See Analog Engineer's Circuit Cookbooks for TI's comprehensive circuit library.
Additional Resources
For direct support from TI Engineers, use the E2E community:
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated