SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
The TAx5xxx-Q1 family of devices are multichannel, high performance, analog-to-digital converters, and codecs intended for automotive audio applications. This application note details the integrated fault diagnostic features of this family and how the family of devices can be used for robust system design.
PurePath is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
Automotive systems are designed to operate in a wide range of harsh environments. As greater amounts of electronics are integrated into automotive systems, the system complexity and potential for faults also increase. Multiple microphones are typically used for automotive audio systems that rely on algorithms like beamforming, active noise cancellation, or speech recognition. These algorithms depend on reliable data from microphones, and if one or more microphones in the system fail, the processing of unreliable data leads to erroneous calculations. In these automotive audio applications, microphones can be placed in remote locations far away from the PCB, such as in a wheel well, close to the engine, or at different positions in the passenger cabin. The remote placement of the microphone makes a wire harness to interface with the rest of the electronics necessary. Although extreme care is taken to prevent failure, over time these harnesses can degrade, resulting in faulty microphone connections. The new family of automotive audio data converters from Texas Instruments helps to address this challenge by providing integrated diagnostic monitoring features that determine when an input fault condition has occurred. With this information, the system can select how to respond and adjust system algorithms to handle the error.