This user's guide is a quick reference to the features and options of the of the KDK350ADPTR-EVM. Topics include using the EVM, header pinout, backlight control, LCD interface control switches, and touchscreen interface.
SimpleLink, Code Composer Studio are trademarks of Texas Instruments.
Arm is a registered trademark of Arm Limited.
IAR Embedded Workbench is a registered trademark of IAR Systems.
All other trademarks are the property of their respective owners.
The KDK350ADPTR-EVM provides a physical adapter layer to interface the MSP432E411Y microcontroller (MCU) on the SimpleLink™ Ethernet MSP432E411Y MCU Evaluation Board (MSP432E411Y-BGAEVM) to a Kentec Display K350QVG-V2-F-04 LCD, including the LCD backlight driver. The KDK350ADPTR-EVM can be used as a reference for connecting other LCD modules to the MSP432E411Y-BGAEVM.
The Kentec Display K350QVG-V2-F-04 LCD is a 3.5-inch diagonal, 320-×240-pixel resolution, TFT module display that has LED backlighting and supports the i80 8-, 16-, or 18-bit interface and SPI. The display also includes an integrated resistive touch panel.
Figure 1 shows the KDK350ADPTR-EVM with key features highlighted.
The KDK350ADPTR-EVM is used with the MSP432E411Y-BGAEVM to showcase the 16-bit parallel LCD interface on the MSP432E411Y device. The SimpleLink MSP432E4 Software Development Kit (SDK) includes a graphics library example of the LCD capabilities of the MSP432E411Y MCU.
To use the KDK350ADPTR-EVM with an MSP432E411Y-BGAEVM and the graphics library example, follow these steps: