This user's guide provides an overview of the features and options of the BOOSTXL-SHARP128, including power, header pinouts and connections, and communication interfaces.
BoosterPack, LaunchPad, SimpleLink, MSP430Ware, Code Composer Studio, E2E are trademarks of Texas Instruments.
Arm, Keil, RealView are registered trademarks of Arm Limited.
IAR Embedded Workbench is a registered trademark of IAR Systems.
Sharp is a registered trademark of Sharp Microelectronics.
The Sharp® 128x128 Memory LCD and microSD Card TI BoosterPack™ Plug-in Module (BOOSTXL-SHARP128) is based on the LS013B7DH03 super-low-power TFT display panel from Sharp Electronics and also features a microSD card expansion slot. Both the LCD and SD card can be controlled using the serial peripheral interface (SPI).
TI MCU LaunchPad™ development kit developers can use this BoosterPack plug-in module to display sensor readings, time, graphics, or other information using the 128-x128-pixel LCD as well as to expand embedded applications with SD card read/write capabilities.
NOTE
The BOOSTXL-SHARP128 supersedes the obsoleted 430BOOST-SHARP96, which used the discontinued Sharp LS013B4DN04 LCD module. The 128x128 LS013B7DH03 and the 96x96 LS013B4DN04 LCD modules are pin-to-pin compatible with reusable firmware and drivers.