Advisories that affect factory-programmed software.
✓ The check mark indicates that the issue is present in the specified revision.
The device does not have any errata for this category.
Advisories that affect only debug operation.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev A |
---|---|
EEM20 | ✓ |
Advisories that are resolved by compiler workaround. Refer to each advisory for the IDE and compiler versions with a workaround.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev A |
---|---|
CPU4 | ✓ |
Refer to the following MSP430 compiler documentation for more details about the CPU bugs workarounds.
TI MSP430 Compiler Tools (Code Composer Studio IDE)
MSP430 GNU Compiler (MSP430-GCC)
IAR Embedded Workbench