Advisories that affect the device's operation, function, or parametrics.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev K | Rev I | Rev H | Rev G | Rev F | Rev E | Rev D | Rev C |
---|---|---|---|---|---|---|---|---|
ADC25 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | |
ADC27 | ✓ | ✓ | ✓ | |||||
ADC29 | ✓ | |||||||
ADC42 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
ADC69 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
COMP10 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU37 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU47 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
DMA4 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
DMA7 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
DMA8 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
DMA10 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
FLASH33 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
FLASH34 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
FLASH35 | ✓ | ✓ | ||||||
FLASH37 | ✓ | ✓ | ✓ | |||||
MPY1 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMAP1 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM9 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM10 | ✓ | ✓ | ✓ | |||||
PMM11 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM12 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM14 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM15 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM17 | ✓ | ✓ | ✓ | |||||
PMM18 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PMM20 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PORT15 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PORT16 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PORT19 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
PORT24 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
RTC3 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
RTC6 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
SYS10 | ✓ | ✓ | ✓ | |||||
SYS12 | ✓ | ✓ | ✓ | |||||
SYS14 | ✓ | ✓ | ✓ | |||||
SYS16 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
TAB23 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI26 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI30 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI31 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI34 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI35 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI39 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
USCI40 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
WDG4 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
Advisories that affect only debug operation.
✓ The check mark indicates that the issue is present in the specified revision.
Advisories that are resolved by compiler workaround. Refer to each advisory for the IDE and compiler versions with a workaround.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev K | Rev I | Rev H | Rev G | Rev F | Rev E | Rev D | Rev C |
---|---|---|---|---|---|---|---|---|
CPU21 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU22 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU23 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU26 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU27 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU28 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU29 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU30 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU31 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU32 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU33 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU34 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU35 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU39 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
CPU40 | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ | ✓ |
Refer to the following MSP430 compiler documentation for more details about the CPU bugs workarounds.
TI MSP430 Compiler Tools (Code Composer Studio IDE)
MSP430 GNU Compiler (MSP430-GCC)
IAR Embedded Workbench