The BQ27Z746EVM comes with the BQ27Z746 integrated gas gauge and protection IC with external high-side protection N-Channel FETs. This user's guide will walk you through the following tasks:
These tasks will guide users of the BQ27Z746EVM through the process required to prepare for production with the BQ27Z746 by creating a "Golden Pack". A Golden Pack is a single gauge and battery that has had optimization and configuration processes performed on it during the development stage. The resulting values are extracted from the Golden Pack gauge into the “Golden File” or “Golden Image”. The Golden File is a flash image programmed into every gauge used in mass production as there should be minimal pack-to-pack variation during a well-controlled manufacturing process. The Impedance Track™ algorithm enables the gauge to continue to learn once a pack is deployed to account for manufacturing differences, field conditions, and battery degradation over its lifetime.