All trademarks are the property of their respective owners.
The TPSI3050-Q1 is a fully integrated isolated switch driver, which when combined with an external power switch, forms a complete isolated solid state relay solution. With a nominal gate drive voltage of 10 V 1.5-A peak source current and 3-A peak sink current, a large variety of external power switches can be chosen to meet a wide range of applications.
The following summarizes known errata.
Errata Number | Description |
---|---|
1 | In two-wire mode, under some conditions, the falling edge of EN can not be recognized, leading to VDRV being asserted low after a duration of tHL_VDRV_PD. |