SPRADK6 September 2024 TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Nowadays, topologies that requiring PWM phasing-shifting and frequency-changing have been widely used in digital power applications. Complicated topologies like multi-phase interleaved LLC have been introduced as the result of demand for higher efficiency and higher power level. To handle the challenge, Type-4 PWM is introduced on TI generation 3 C2000 devices. Especially, new features like global load and one shot reload would significantly simplify implementation phase-shifting and frequency changing topology. This application note discusses the benefit of these new features, and how to deal with corner cases in real practice.
All trademarks are the property of their respective owners.
With higher requirement of power rating and efficiency in power applications like server and telecom PSU, resonant converters like LLC have become the prioritized option of DC/DC stage in more and more new designs. Comparing with traditional full-bridge topology, LLC is easier to achieve soft switching due to resonant operation, leading to better EMI performance, higher efficiency and less stress on power stage.
Normally the LLC converter works under variable frequency but fixed duty cycle. The typical gain curve of a LLC converter is shown in the following picture. The converter works near frand adjust switching frequency through the control loop to stabilize the output voltage.