All trademarks are the property of their respective owners.
The Jacinto7 EVMs are development and evaluation systems that enable developers to write software and develop hardware around the Jacinto7 family of processors. The main elements of the system are available on the base board(s) of the EVM. This gives developers the basic resources needed for most general-purpose type projects that encompass the Jacinto7 processor.
The Jacinto7 EVM is comprised of two boards:
Beyond the basic resources provided, additional functionality can be added via expansion cards.
This technical user's guide describes the hardware architecture and functionality of the Gateway/Ethernet Switch/Industrial (GESI) expansion board.
Below are the key features of the expansion board:
Jacinto7 EVM can support different types of expansion boards. Not all of the expansion boards are supported on each Jacinto7 EVMs.
To determine which version Jacinto7 EVM supports the GESI expansion board, see Section A.
Figure 2-1 shows the overall architecture of Jacinto7 EVM.