SPRUJ96A November 2023 – April 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
Flash is an electrically erasable/programmable non-volatile memory that can be programmed and erased many times to ease code development. Flash memory can be used primarily as a program memory for the core, and secondarily as static data memory. This guide describes the usage of the flash API library to perform erase, program and verify operations for the on-chip Flash memory of TMS320F280013x/15x devices.
Arm® is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
All trademarks are the property of their respective owners.
This reference guide provides a detailed description of both the Texas Instruments TMS320F280013x Flash API Library (FAPI_F280013x_EABI_v2.00.10.00 & FAPI_F280013x_COFF_v2.00.10.00) and TMS320F280015x Flash API Library (FAPI_F280015x_EABI_v2.00.10.00 & FAPI_F280015x_COFF_v2.00.10.00) functions that can be used to erase, program and verify Flash on TMS320F280013x/15x devices. Even though the library names for TMS320F280013x/15x are different, the Flash API libraries are same. Note that the Flash API V2.00.XX.XX should be used only with TMS320F280013x/15x devices. The Flash API Library for TMS320F280013x is provided in C2000Ware at C2000Ware_x_xx_xx_xx\libraries\flash_api\f280013x. The Flash API Library for TMS320F280015x is provided in C2000Ware at C2000Ware_x_xx_xx_xx\libraries\flash_api\f280015x.