Table 1-1 lists all usage notes and the applicable silicon revision(s). Table 1-2 lists all advisories, modules affected, and the applicable silicon revision(s).
Module | DESCRIPTION | SILICON REVISIONS AFFECTED | |
---|---|---|---|
AM263x | |||
1.0A | 1.1 | ||
CLOCKS | i2324 — No synchronizer present between GCM and GCD status signals | YES |
YES |
QSPI | i2364 — QSPI: Access to address beyond 8MB is not supported in mem map mode | YES | YES |
VDDA | i2348 — VDDA1V8 Static Power leakage | YES |
NO |
MODULE | DESCRIPTION | SILICON REVISIONS AFFECTED | |
---|---|---|---|
AM263x | |||
1.0A | 1.1 | ||
ADC | i2346 — ADC result has Error when switching between odd and even channels | YES |
NO |
ADC | i2347 — VREF current consumption of ADC is random at powerup | YES |
NO |
ADC | i2349 — ADC VrefHi Loading increase in powerdown | YES | NO |
CONTROLSS | i2352 — CONTROLSS-SDFM: Dynamically Changing Threshold Settings (LLT, HLT), Filter Type, or COSR Settings Will Trigger Spurious Comparator Events | YES | YES |
CONTROLSS | i2353 — CONTROLSS-SDFM: Dynamically Changing Data Filter Settings (Such as Filter Type or DOSR) Will Trigger Spurious Data Acknowledge Events | YES | YES |
CONTROLSS | i2354 — CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events | YES | YES |
CONTROLSS | i2355 — CONTROLSS-ADC: DMA Read of Stale Result | YES | YES |
CONTROLSS | i2356 — CONTROLSS-ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set | YES | YES |
CONTROLSS | i2357 — CONTROLSS-ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window | YES | YES |
CONTROLSS | i2358 — CONTROLSS-ePWM: Trip Events Will Not be Filtered by the Blanking Window for the First 3 Cycles After the Start of a Blanking | YES | YES |
CONTROLSS | i2359 — CONTROLSS-CMPSS:Prescaler counter behavior different from spec when DACSOURCE is made 0 or reconfigured as 1 | YES | YES |
CONTROLSS | i2405 — CONTROLSS: Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss | YES | YES |
CPSW | i2345 — CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks | YES | YES |
CPSW | i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up | YES | YES |
CPSW | i2402 — CPSW: Ethernet to Host Checksum Offload does not work | YES | YES |
CPSW | i2438 — CPSW - Host to Ethernet Checksum Generation with VLAN ADD/Remove | YES | YES |
CPSW | i2439 — CPSW: Host to Ethernet Timestamp Accuracy Issue | YES | YES |
CRC | i2386 — CRC: CRC 8-bit data width and CRC8-SAE-J1850 and CRC8-H2F possible use in CAN module is not supported | YES | YES |
DCC | i2395 — DCC Module Frequency Comparison can Report Erroneous Results | YES | YES |
GPMC | i2313 — GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO | YES | YES |
M4 ROM | i2403 — M4 ROM: SBL redundant boot image feature not supported on HSSE devices | NO | YES |
MBOX | i2404 — MBOX: Race condition in mailbox registers resulting in events miss | YES | YES |
McSPI | i2350 — McSPI data transfer using EDMA in ‘ABSYNC’ mode stops after 32 bits transfer | YES | YES |
MDIO | i2329 — MDIO interface corruption (CPSW and PRU-ICSS) | YES | NO |
PBIST | i2374 — PBIST fails if clock frequency of R5SS_CORE_CLK is not same as R5FSS_CLK_SELECTED frequency | YES | YES |
SOC CONTROL | i2392 — Race condition in mem-init capture registers resulting in events miss | YES | YES |
BUS SAFETY | i2393 — Granular error status not logged in BUS_SAFETY_ERR registers for the detected faults | YES | YES |
SOC CONTROL | i2394 — Race condition in interrupt and error aggregator capture registers resulting in events miss | YES | YES |
SFDM | i2375 — SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected | YES | YES |
UART | i2310 — USART: Erroneous triggering of timeout interrupt | YES | YES |
UART | i2311 — USART: Spurious DMA Interrupts | YES | YES |
RAM SEC | i2427 — RAM SEC can cause Spurious RAM writes resulting in L2 & MBOX memory corruption | YES | YES |
AES | i2428 — AES in DTHE generates extra dma request for data_in at the end of GCM encrypt | YES | YES |
ICSS | i2433 — ICSS: Reading the 64-bit IEP timer does not have a lock MSW logic when LSW is read | YES | YES |
CPSW | i2438 — CPSW: Host to Ethernet Checksum Generation with VLAN ADD/Remove | YES | YES |
CPSW | i2439 — CPSW: Host to Ethernet Timestamp Accuracy Issue | YES | YES |
No synchronizer present between GCM and GCD status
signals
There is no synchronizer in between GCM and GCD, so the clock configuration register reads may be incorrect momentarily.
Minor
Poll for the status registers change until it reflects the programmed SRC_SEL and DIV values.