Gen Vansteeg
Imagine a robot arm bending and turning, each of its axes equipped with beautifully precise motor drives, sensors and perhaps machine vision – a symphony of movement. But if the conductor wasn’t there to tell each part of the system how and when to perform its role, that robot arm could devolve into a cacophony of clashing and grinding metal.
In previous editions of our real-time control series, we’ve talked about the instruments of real-time control (RTC): sensing, actuation and processing. The last piece needed to pull it all together is the conductor: real-time communications. In this article, I will use Industry 4.0 as the basis for the discussion because it is predicated on real-time communication and control.
COVID-19 demonstrated that factory operation without human intervention is highly coveted. The collection and appropriate distribution of big data (defined by the Oxford Dictionary as extremely large data sets that may be analyzed computationally to reveal patterns, trends and associations, especially relating to human behavior and interactions) enables digital twinning, metering, service charges and predictive maintenance. For example, having big data available allows for the monitoring of a robot arm’s performance and system health alongside data rates, temperature, moisture, vibration, etc., enabling the development of models (digital twins) that will be able to predict future performance and health based on AI, which uses big data to learn. To take advantage of these benefits, it’s necessary to converge information technology (IT) and operational technology (OT), and so support the Internet Protocol (IP) all the way to the edge of an RTC system. Logically, this is known as the convergence of IT and OT.
In Ethernet, the network and transport layers of the Open Systems Interconnection (OSI) model enable the Transmission Control Protocol/Internet Protocol (TCP/IP), and so Ethernet inherently supports IPv4 (and IPv6). The ability to deterministically communicate the required volumes of information, while inherently supporting IPv4, is why industrial Ethernet is becoming the de facto communication standard in industrial automation convergence. Legacy fieldbuses presently remain in place to communicate with edge devices because the existing infrastructure often uses two-wire protocols without native TCP/IP capability. Figure 1 represents communications in industrial automation today.
Industrial communications implementations are starting to change. Single-pair Ethernet (SPE) can maintain existing two-wire system architectures while also supporting the faster speeds and benefits of industrial Ethernet. Advanced in situ diagnostics support both distributed and centralized monitoring and actions. And of course, SPE is able to reuse the existing two-wire infrastructure established by multiple existing fieldbuses, simplifying and minimizing the cost of convergence-driven upgrades.
While open and ubiquitous in enterprise applications, until recently it was not possible to use Ethernet in real-time applications because the delivery of IT Ethernet frames was “best effort” and unmanaged; errors, even in the best case, are annoying. In real-time OT, errors can be catastrophic, or worse, dangerous. RTC systems need reliable communications as the system’s conductor to ensure that the system operates as expected, avoiding mismanufactured products or causing system damage or human injury. Environmental challenges for IT Ethernet are rare, as IT Ethernet is generally used in an enterprise or consumer environment. Conversely, RTC systems are often located in harsh environments.
The need for robust, deterministic behavior, such as reliability in wide-temperature, noisy and dirty environments, along with higher data rates, drove the advent of industrial Ethernet. Industrial Ethernet is deterministic, robust and capable of providing both the additional bandwidth and inherent IP connectivity to get the most from RTC systems.
Let’s talk about timing characteristics and how they apply to Ethernet physical layers (PHYs).
There are three main timing characteristics important in RTC systems:
Industry 4.0 depends on the successful deployment of RTC and communications. And it isn’t just Industry 4.0 – by using deterministic, synchronized and low-latency communication PHYs and industrial Ethernet protocols, all the instruments of the world can begin to make beautiful music together.