Sam Wallace
Other Parts Discussed in Post: LM3880-Q1, UCD9090-Q1
Over 50 years ago, Moore’s law predicted an exponential increase in technological advancement; cars were never exempt from this. In just the last five years, we have seen advancements such as lane-keeping assist, early autonomous driving, and all manner of other safety and convenience features. The one thing all of these features have in common is that they need to be powered. The process of doing so is becoming more and more complex, as more sensors and more features are added.
One requirement of an increasingly complex power tree is the need to turn different rails on in a specific order, especially in relation to the processor. A simple way to accomplish this is to use a sequencer integrated circuit (IC), which is a single device that controls the order in which rails power on.
These processors, which run everything from advanced driver assistance systems (ADAS) to head-up displays (HUD), must have their power rails come up in the right order to prevent excessive in-rush current, latch-up conditions, inconsistent internal states and improper initialization. Going the other way issues such as corrupted memory, improperly biased diodes and other system damage can result if the power-supply rails shut down in the wrong order. Figure 1 is an example of the necessary power-up sequence of rails on a field-programmable gate array (FPGA) from the Intel Stratix 10 Power Management User Guide.
As I mentioned, you could implement this required power-up order with a sequencer IC, such as TI’s LM3880-Q1 and UCD9090-Q1; another popular method is a discrete solution. A typical discrete solution uses a resistor-capacitor (RC) network with some diodes to create a delay on the enable of each rail. The values of these components will create the desired order in which these rails will be enabled. Figure 2 shows an example of this implementation.
Compared to a sequencer IC, a discrete implementation is likely to be cheaper and use less board space; however, they also have several drawbacks. A discrete solution will provide only power-up sequencing, not power-down sequencing. Discrete solutions are also less precise than a dedicated sequencer IC, as discrete components must deal with the usual component tolerances as well as temperature variations.
A sequencer such as the LM3880-Q1 has almost no variation in delay between rails due to varying temperature conditions so often found in automotive applications. Sequencers are also easier to implement and design than discrete solutions. In fact, the LM3880-Q1 requires no external components and can replace over 10 discrete components in a three-rail system, leaving less opportunity for manufacturing discrepancies and errors.
Figure 3 shows an implementation of a sequencer in the Cost-Optimized Power-Supply Solution for Entry-Level Core Application Processor-Based ADAS Systems reference design.
All of these drawbacks mean that a discrete solution for sequencing is more likely to lead to accidental damage to your processor or even just increased stress, leading to a decrease in its lifespan. When considering the difficulty of repairing or replacing electronic systems in vehicles, this directly relates to the vehicle’s lifespan.
Altogether, a sequencer IC solution is going to be more reliable, more effective and easier to implement than a discrete sequencing solution. In automotive applications this is crucial, as these systems require reliable, efficient, long-lasting solutions. Learn more about TI’s ADAS and hybrid/electric powertrain systems.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated