RJ Hopper
** This is the 10th post in an Analog Wire RF-sampling blog series. **
In my previous blog post, I discussed the advantages of radio-frequency (RF) sampling architectures for wide-bandwidth systems, but some systems operate with moderate bandwidth requirements or have other key considerations. Active antenna arrays use multiple antennas specifically distributed to create a more focused radiation pattern than what’s possible with a single element. This focused pattern increases the antenna gain to the intended target or user while simultaneously providing interference rejection to areas outside the beam pattern, and thus does not require excessive signal bandwidth.
Radar array is one example of an active antenna system used to pinpoint the location of a target in space. The radar-array system depicted in Figure 1 illustrates a simple three-by-three array capable of steering the beam in two dimensions to track a target.
Each antenna element requires its own receiver. Smaller arrays may use eight elements; very large arrays use thousands of elements. With so many receivers required for these systems, it is imperative that each receiver be low cost and power-efficient; however, these systems still require high dynamic-range capabilities to discern the target from the background noise and interference.
The TI Designs 700-2700MHz Dual-Channel Receiver with 16-Bit ADC and 100MHz IF Bandwidth Reference Design (TIDA-00360) showcases the TSW16DX370 evaluation module (EVM) which is a super-heterodyne receiver applicable for active antenna-array systems. Figure 2 shows the block diagram. This reference design uses the TRF37B32 dual mixer to convert input RF signals to an intermediate frequency (IF). The mixer has excellent gain, noise figure and input-linearity performance for any high-end communication system. The TRF37B32 achieves its performance at one of the lowest power-dissipation levels of similar devices. This is critical when the system must employ dozens to hundreds of receivers.
In normal operation, the device consumes about 1W per channel (at 1,950MHz). Current consumption is dependent on local oscillator (LO) frequency. If you need further power reduction, the TRF37B32 offers a low-power mode that drops the nominal dissipation to 0.6W per channel at 1,950MHz. There is also an option to independently power down each branch if you need only a single channel or power down both channels for time-division duplexing (TDD) operation.
The TSW16DX370EVM includes an IF band-pass filter centered around 250MHz with a 1dB bandwidth of 100MHz.The EVM incorporates the ADC16DX370 analog-to-digital converter (ADC), which provides 16-bit resolution and operates at 370MSPS. It offers the signal-to-noise performance required for discerning small signals from background noise and uses the JESD204B standard for serializing digital data. The ADC16DX370 uses as few as two lanes to transfer all of the data from two converters to a centralized processor. When dealing with many receivers, it is advantageous to condense the digital interface to minimize routing.
The focused beam is of limited use without the ability to steer the beam where needed. Modifying the relative phase of each element using an inline phase-adjustment circuit steers the beam. Figure 3 shows a varactor-based analog phase-adjuster circuit. The hybrid coupler keeps the input and output return loss at reasonable levels. If the signal path includes the circuit, RF performance (particularly intermodulation distortion) degrades because of the varactor’s nonlinear performance.
An alternative approach is to place the phase-adjuster circuitry in the LO path (as shown in Figure 4) where the signal is a single-frequency sinusoid and not a modulated signal. This achieves the desired phase adjustment without impacting noise or linearity performance as a function of adjustment voltage.
The proposed receiver maintains high performance at low power dissipation that easily scales to any size antenna array.
Check back next month where I discuss a receiver solution for capturing 1-GHz bandwidth signals.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated