WiLink is a trademark of Texas Instruments.
Litepoint and IQxel are trademarks of LitePoint Corporation.
FTDI is a trademark of Future Technology Devices; International Limited.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
Pentium is a registered trademark of Intel Corporation.
Windows is a registered trademark of Microsoft Inc..
Bluetooth is a registered trademark of Bluetooth SIG.
Android is a registered trademark of Google, Inc.
Linux is a registered trademark of Linus Torvalds.
All trademarks are the property of their respective owners.
The RTTT requires the following hardware and software:
Debug and calibration tools for WLAN and Bluetooth® require four UART ports. The most efficient way to drive these ports to the PC is to use a UART-to-USB converter (not included in the wireless tools package). TI recommends using the WL18XXCOM82SDMMC adapter with the TI WL1837MODCOM8I module or WL1835MODCOM8B module on the COM8 board.
Multiple UART-to-USB adapters are available on the market, such as the FTDI™ Chip development modules.