Publication date: June 13, 2022
CVEID: None
Summary
The CC13x0 SimpleLink connected microcontrollers contain an Elliptic Curve Cryptography library in ROM. The following input validations are not present in the ROM library:
Missing Validation | Validation Defined by | Impacted Functions |
---|---|---|
Public key point is not the identity element | NIST SP 800-56A Rev 3, section 5.6.2.3.3 |
ECC_ECDH_computeSharedSecret, ECC_ECDSA_verify |
Public key points are in the range [0, p - 1] | NIST SP 800-56A Rev 3, section 5.6.2.3.3 | |
Public key point is on the curve | NIST SP 800-56A Rev 3, section 5.6.2.3.3 | |
r and s portions of signature are in range [1, n – 1] | ANS X9.62-2005, section 7.4 | ECC_ECDSA_verify |
Per message secret is in range [1, n – 1] | FIPS PUB 186-4, section 6.3 | ECC_ECDSA_sign |
Private key is in range [1, n – 1] | NIST SP 800-56A Rev 3, section 5.6.2.1.2 | ECC_generateKey |
In addition, example code included in the CC1310 and CC1350 SDK incorrectly generated entropy used as an input to ECDSA sign operations, resulting in reduced protection of the private key material.
CVSS base score: 6.5
CVSS vector: CVSS:3.1/AV:A/AC:L/PR:N/UI:N/S:U/C:H/I:N/A:N
Affected products and versions
Part | SDK Versions | Version |
---|---|---|
CC1310, CC1350 | SimpleLink™ Sub-1 GHz CC13x0 Software Development Kit | version 4.20.01.03 and earlier |
While some newer parts in the CC13XX series of SimpleLink microcontrollers also contain a ROM library for ECC operations, the ROM in those newer devices do perform these input validations.
Potentially impacted features
The following are potential impacts:
Suggested mitigations
Customers are encouraged to upgrade to the latest SDK for CC1310 and CC1350. The impacted functions are now provided with wrappers in source code to validate the inputs prior to calling the functions in ROM.
If customers desire to limit when the validation is performed, new functions have been provided which do not perform the validation. Skipping the validation may be desirable as the validation steps increase the time to perform the operations. Customers are encouraged to always validate the inputs at least once (for example, validate keys on first use and then store the validated keys in non-volatile memory with integrity protections for subsequent uses.)
In addition, customers are encouraged to confirm that ECC private key material is in the range [1, n -1] before using the private key in any operations. This can be done by using the updated ECC_generateKey() function.
Finally, if customers based their application code on the “aesKeyAgreement” example included in the SDK, customers should review their code to ensure calls to ECC_ECDSA_sign() are performed correctly. Check that the 3rd parameter passed to ECC_ECDSA_sign(), the randString parameter, is formatted as follows:
For example, when using the NIST P256 curve, the randString parameter should start with: 0x08, 0x00, 0x00, 0x00 and then be followed by 32 bytes of entropy. Consult the updated example code for more details.
The following SDK releases address these vulnerabilities:
SDK | First version with mitigations |
---|---|
SimpleLink™ Sub-1 GHz CC13x0 Software Development Kit | 4.20.02 |
Acknowledgment
We would like to thank Szymon Heidrich of Carrier for reporting this vulnerability to the TI Product Security Incident Response Team (PSIRT).
External References
ANS X9.62, Public Key Cryptography for the Financial Services Industry: The Elliptic Curve Digital Signature Standard (ECDSA), November 2005.
FIPS PUB 186-4, Digital Signature Standard (DSS), July 2013. https://doi.org/10.6028/NIST.FIPS.186-4
NIST Special Publication 800-56A Revision 3, Recommendation for Pair-Wise Key-Establishment Schemes Using Discrete Logarithm Cryptography, April 2018. https://doi.org/10.6028/NIST.SP.800-56Ar3
Revision history
Version 1.0 Initial publication