• Menu
  • Product
  • Email
  • PDF
  • Order now
  • グリッド接続インバータのリファレンス・デザイン

    • JAJU450D November   2015  – March 2020

       

  • CONTENTS
  • SEARCH
  • グリッド接続インバータのリファレンス・デザイン
  1.   改訂履歴
  2. 重要なお知らせ
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

DESIGN GUIDE

グリッド接続インバータのリファレンス・デザイン

このリソースの元の言語は英語です。 翻訳は概要を便宜的に提供するもので、自動化ツール (機械翻訳) を使用していることがあり、TI では翻訳の正確性および妥当性につきましては一切保証いたしません。 実際の設計などの前には、ti.com で必ず最新の英語版をご参照くださいますようお願いいたします。

改訂履歴

Changes from C Revision (May 2019) to D Revision

  • Changed powerSUITE Page for the Grid Connected Inverter Solution imageGo
  • Changed Project Explorer View of Solution Project imageGo
  • Changed Current Loop Design Using Compensation Designer imageGo
  • Changed Compensation Designer With Measured Plant Frequency Response Data imageGo
  • Changed SPRUHZ5 to SPRUIK4 linkGo

Changes from B Revision (November 2017) to C Revision

  • Changed TMS310F280049M を TMS310F280049C にGo
  • Added TMS320F280049CGo
  • Changed ブロック図の TMS310F280049M を TMS320F280049C にGo
  • Deleted TMS310F280049M from block diagramGo
  • Changed TMS320F280049M to TMS320F280049CGo
  • Changed <sdk_install_path>\c2000ware\boards\controlcards\TMDSCNCD280049M to <sdk_install_path>\c2000ware\boards\controlcards\TMDSCNCD280049CGo
  • Changed TMS320F280049M to TMS320F280049CGo
  • Changed TMS320F280049M to TMS320F280049CGo

Changes from A Revision (October 2016) to B Revision

  • 現行のデザイン・ガイドのテンプレートに合わせてフォーマットを更新Go
  • Added 「リソース」に TMS320F280049M をGo
  • Added 「特長」に「TMS320F28377D および TMS320F280049M をサポート」をGo
  • Added ブロック図に TMS320F280049M をGo
  • Changed location of Excel sheet of calculationsGo
  • Changed location of info sheet in Section 3.1.1.2: Control Card SettingsGo
  • Added required settings for revision A of the TMS320F280049M control card in Section 3.1.1.2: Control Card SettingsGo
  • Added note in Section 3.1.2: Firmware: powerSUITE and Incremental Build SoftwareGo
  • Changed Step 5 in Section 3.1.2.1: Opening the Project Inside Code Composer Studio™Go
  • Updated Figure 21: Build Level 1 Control Diagram: Open Loop ProjectGo
  • Changed 1.26 VRMS to 1.26 IRMS in Step 13 in Section 3.1.2.3.1.5: Running the CodeGo
  • Updated Figure 26: Build Level 2 Control Diagram: Closed Current LoopGo
  • Changed location of the SFRA.exe file from controlSUITE/libs/app_libs/SFRA/<version>/GUI to <sdk_install_path>/libraries/sfra/GUIGo
  • Changed invloRefInst to invIoRef in Step 46 in Section 3.1.2.3.2.4: Running the CodeGo
  • Deleted the step "Set the clearInvTrip variable to 1 to clear the inverter trip" in Section 3.1.2.3.3.2: Running the CodeGo
  • Added the TMS320F28004x Piccolo™ Microcontrollers Technical Reference Manual to Section 6: Related DocumentationGo
  • Added the TMS320F28004x Piccolo™ Microcontrollers Data Sheet to Section 6: Related DocumentationGo

Changes from * Revision (November 2015) to A Revision

  • Added 「設計リソース」のTIEVM-HV-1PH-DCAC製品ページのリンクGo
  • Added configuration (CFG)Go
  • Added Figure 12: Control Scheme Used for Grid Connected Inverter ControlGo
  • Added note in Section 3: Getting Started With HardwareGo
  • Deleted "Keep in mind that the output capacitor is large (for example, 20 uF)." from Step 2 in Section 3.1: Base Board SettingsGo
  • Changed the control card slot from H5 to J15-J16Go
  • Changed isolated HV DC source connection from CON1 to J17Go
  • Changed Figure 16: Hardware Setup to Run Software for BUILD Level 1Go
  • Added Section 3.3: Tips to Connect JTAG USB CableGo
  • Added Section 4.1.2: Open TI Design Software for AdaptationGo
  • Added "up to 50 V" to Step 9 under Running the CodeGo
  • Added "Now raise the DC Bus voltage slowly up to 380 V" to Step 10 under Running the CodeGo
  • Deleted "Check the frequency of the generated AC waveform." from Running the CodeGo
  • Deleted "Confirm that the generated AC waveform matches the value entered on the powerSUITE page (for example, 60 Hz)." from Running the CodeGo
  • Changed variable from sine_mains.SigFreq to guiFreqAvgGo
  • Changed output voltage from 133 VRMS to 126 VRMSGo
  • Changed current from 1.35 VRMS to 1.26 VRMSGo
  • Changed numeration after Figure 25: BUILD LEVEL 1 Graph1.GraphProp File Showing Measured Per-Unit Voltage and Current ValuesGo
  • Added Figure 27: Hardware Setup to Run Software for Build Level 2: DC CheckGo
  • Deleted "Turn the S1 switch to the ON position."Go
  • Added note under Running the CodeGo
  • Changed title in Figure 32 from "Setup for DC Check of the Current Controller" to "Hardware Setup to Run Software for BUILD Level 2: AC Check"Go
  • Added note after Step 8 in Running the CodeGo
  • Changed Steps 2 through 9 under Running the CodeGo
  • Deleted Steps 10 through 13 under Running the CodeGo
  • Changed Step 16 under Running the CodeGo

重要なお知らせと免責事項

TI は、技術データと信頼性データ(データシートを含みます)、設計リソース(リファレンス・デザインを含みます)、アプリケーションや設計に関する各種アドバイス、Web ツール、安全性情報、その他のリソースを、欠陥が存在する可能性のある「現状のまま」提供しており、商品性および特定目的に対する適合性の黙示保証、第三者の知的財産権の非侵害保証を含むいかなる保証も、明示的または黙示的にかかわらず拒否します。
これらのリソースは、TI 製品を使用する設計の経験を積んだ開発者への提供を意図したものです。(1) お客様のアプリケーションに適した TI 製品の選定、(2) お客様のアプリケーションの設計、検証、試験、(3) お客様のアプリケーションが適用される各種規格や、その他のあらゆる安全性、セキュリティ、またはその他の要件を満たしていることを確実にする責任を、お客様のみが単独で負うものとします。上記の各種リソースは、予告なく変更される可能性があります。これらのリソースは、リソースで説明されている TI 製品を使用するアプリケーションの開発の目的でのみ、TI はその使用をお客様に許諾します。これらのリソースに関して、他の目的で複製することや掲載することは禁止されています。TI や第三者の知的財産権のライセンスが付与されている訳ではありません。お客様は、これらのリソースを自身で使用した結果発生するあらゆる申し立て、損害、費用、損失、責任について、TI およびその代理人を完全に補償するものとし、TI は一切の責任を拒否します。
TI の製品は、TI の販売条件(www.tij.co.jp/ja-jp/legal/termsofsale.html)、または ti.com やかかる TI 製品の関連資料などのいずれかを通じて提供する適用可能な条項の下で提供されています。TI がこれらのリソースを提供することは、適用されるTI の保証または他の保証の放棄の拡大や変更を意味するものではありません。IMPORTANT NOTICE
Copyright © 2020, Texas Instruments Incorporated
日本語版 日本テキサス・インスツルメンツ株式会社

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale