DLPA073A September 2016 – September 2016 DLP2010 , DLPC2607 , DLPC3430 , DLPC3435
The desired virtual image distance (VID) is typically within the range of 2.4 meters to 30 meters (8 ft to 98 ft) so that the HUD presents information at the normal sight distance of vision during driving. A 3° down angle is also recommended for the virtual image so that the driver does not have to move their attention away from the lane of traffic in order to see information. The VID has no impact on the total light output from the projection unit, or the resolution required for the HUD. The virtual image position is determined by the HUD optical design.