DLPS228D October 2021 – October 2024 DLP160CP
PRODUCTION DATA
For instructions on how to connect the DLPC3421 controller, the DLPA200x/DLPA3000, and the DLP160CP DMD together, see the reference design schematic. When a circuit board layout is created from this schematic a very small circuit board is possible. An example small board layout is included in the reference design data base. Layout guidelines should be followed to achieve a reliable projector.
The optical engine that has the LED packages and the DMD mounted to it is typically supplied by an optical OEM who specializes in designing optics for DLP projectors.