The DLPC910 Mirror Float command should not be used!
After the first instance of the Mirror Float command, all subsequent use of either PWR_FLOAT or Mirror Float commands will not execute correctly.
This issue will cause the DLPC910 to incorrectly power down the DMD when the PWR_FLOAT command is asserted as required to correctly power down the DMD.
This issue is currently in firmware versions 1.0 and 2.0 of the DLPR910 (DLPR910 & DLPR910A).