DLPU018J October 2014 – June 2024 DLPC900
To execute a command to read the Input Data Channel Swap setting, the host builds a sequence of bytes containing the Secondary address, the sub-address, and the data (if any), and performs the following steps:
An example of the above read command sequence is shown in Table 1-2, and a waveform diagram of a host executing this read sequence is shown in Figure 1-1 and Figure 1-2.
SECONDARY ADDRESS | SUB-ADDRESS | DATA | |||
---|---|---|---|---|---|
0x34 | 0x04 | ||||
0x35 | 0x03 |