C Revision History
Changes from Revision I (November 2023) to Revision J (June 2024)
- Added tables and information about DMD Communication FaultGo
- Corrected bit counts and corrected Pixel Clock frequency units to kHz in Parallel Port Configuration
Go
- Updated minimum exposure time for active block 16 (DLP5500) and active block 6 (DLP670S) in Table 2-109
Go
- Updated the DLP5500 DMD minimum pattern time for bit depth 3 and 6 in Table 2-110
Go
- Debug Mode Commands addedGo
- Added Destination Controller, DLPA200 Status, DMD Communication Status, and Debug commands in I2C Register Quick Reference
Go
- Added Destination Controller, DMD Communication Status, and Debug commands in Command Guide.Go
- Added Destination Controller, Memory Read/Write and Debug Mask commands in Command Descriptors
Go
Changes from Revision H (July 2022) to Revision I (November 2023)
- Updated
the
Related
Documents Table (added DLP5500 DMD and DLPLCR55EVM)Go
- Updated
links
in
If
You Need
Assistance
Go
- Added note to clarify I2C bit structureGo
- Added tables and information about DLPA200 Status and DLPA200 FaultGo
- Added reference to Section 2.3.1.2.Go
- Changed Title to DMD Park/Unpark (No Longer
Recommended)Go
- Added table to clarify the use of Idle and Standby modes and edited
the paragraph to reflect the table informationGo
- Added clarifying information about
Single Pixel and Dual Pixel modesGo
- Updated Single DLPC900 and Dual DLPC900 Block Diagrams to match
DLPC900 Data Sheet [DLPS037]Go
- Updated
input display resolution command definition descriptions for byte 5:4 and 7:6 in
Table 2-99 by changing from vertical/horizontal to horizontal/vertical,
respectivelyGo
- Added DLP5500 DMD Block Load Minimum Exposure Rates tableGo
- Added DLP5500 to Minimum Exposure TableGo
- Number of LUT entries depends on DMD - 960 for DLP5500 and 400 for all other DMDsGo
- Replaced exact timing with link to the Minimum Exposure Times in Any Pattern Mode tableGo
- Pattern Index range depends on DMD - 0 up to 959 for DLP5500 and 0
up to 399 for all other DMDsGo
- DMD Idle Mode can also be started from Video Mode.Go
- Added command supporting DLPA200 Status and DLPA200 FaultGo
Changes from Revision G (April 2022) to Revision H (July 2022)
- Changed Start Address Command description type to
write.Go
- Added note that this I2C sub-address also exists in the
main application as Read Error Code.Go
- Added note that this
I2C sub-address also exists in the main
application as Read Error Description.Go
- Added note that the batch file delay command cannot be used to wait
for Vsync lock.Go
- Changed the description of the second control byte from COLOR BYTE
to CONTROL BYTE 2,Go
- Removed extraneous last line of RLE Compression
Example.Go
- Corrected Control Bytes End of
Line and added Control Bytes for End of
Image.Go
- Changed last line of Enhanced RLE Compression Example to show "End-of-Image command".Go
- Corrected note reference to
pattern stop/start command to 0xE5 in Pattern Display Commands
Go
- Changed minimum trigger 1 delay to refer to DMD Block Load Minimum Exposure Times
Go
- Corrected Pattern On-The-Fly Example command sequenceGo
- Clarified that the command list does not include
programming commands in DLPC900 Firmware Programming Commands.Go
- Corrected USB address for command for Get Minimum LED Pattern Exposure in μs in the Command Matrix
Go
- Added missing Get Minimum LED Pattern Exposure in ns command in the Command Matrix
Go
- Added missing Input Source Configuration Command in the Command Matrix
Go
- Added missing I2C command for Get Minimum LED Pattern Exposure in μs in the Command Matrix
Go
- Added missing I2C command for Get Minimum LED Pattern Exposure in ns in the Command Matrix
Go
- Removed I2C read command 0x65 listed for Pattern Start/Stop command in the Command Matrix
Go
- Corrected Pattern LUT Reorder Configuration USB Command to 0x1A32 in the Command Matrix
Go
Changes from Revision F (December 2020) to Revision G (April 2022)
- Changed all instances of legacy terminology to "Primary" and
"Secondary" throughout this guide.Go
- Harmonized all hexadecimal values to the format 0xh where
h is a value consisting of hexadecimal digits.Go
- Changed Note to point to Table 2-19 for areas that should not be erased.Go
- Clarified Standby mode description.Go
- Added note that the only command during Standby is a return to
normal operation is accepted. Other commands may result in unexpected
behavior.Go
- Updated Single DLPC900 and Dual DLPC900 Block Diagrams with proper
Voltage notation, Primary and Secondary DLPC900s, and Cables instead of
FLEX.Go
- Removed TI component part number from Block Diagrams and added links
to the Single DLPC900 EVM and Dual DLPC900 EVM design files for current TI
component numbers.Go
- Clarified which interfaces belong to each of the three Pattern
Modes.Go
- Added note for use of stop
commandGo
- Updated description of byte 5:2Go
- Updated description of byte 5:2Go
- Byte 5:2 information for Play Once vs RepeatGo
- Changed LLFAULT_ terms to category
descriptionsGo