DLPU018J October 2014 – June 2024 DLPC900
The batch file name command returns the name of the given batch file index and is useful for listing the set of batch files available for the user to execute. To list all the batch file names, iterate through all numbers from 0 to n until an error is returned, which identifies the end of the list.
I2C | USB | |
---|---|---|
Read | 0x1A14 | |
0x3A |
BYTES | BITS | DESCRIPTION | RESET | TYPE |
---|---|---|---|---|
0 | 7:0 | Batch Command Index (Read parameter) | d0 | w |
15:1 | All | Batch Command Name String (Read result) | d0 | r |