DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
The DLPC230-Q1 is the host controller of a SPI communication interface with the TPS99000-Q1. This SPI protocol uses 9-bit bytes with one parity bit per byte. Each write and read transaction returns the parity error status from the TPS99000-Q1. The returned parity error status and the parity of the returned bytes must be correct for the command to be considered successful. If 3 consecutive frames of commands fail, the main application will take action.