Flash parameters are used to specify:
- Current Limit Percentage Threshold - If the LED current is measured above this percentage of the current limit, the LED will be assumed to be operating at the current limit.
- LED Current Minimum - If the LED current is measured below this milliamp value, the LED is considered to be operating at its minimum current.
- Frame Threshold - Number of consecutive frames over which the failure condition must be met in order to be considered to take failure action. This is used to filter out potential instantaneous noise in measurements and avoid false failures.
- TIA Output Voltage Minimum - If the TIA voltage is measured below this voltage value, the TIA is considered to be at minimum output.
- LED Anode Voltage Threshold - Voltage threshold for LED to be considered at maximum voltage.