DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
If the error is a system voltage error, then the information bits will provide the value of the invalid voltage that was detected.
These errors include 843, 844, 845, 846, 847, 848, 849, 1008, 1015.
BITS | DESCRIPTION |
---|---|
15:0 | Error voltage level Absolute value of the measured floating point value converted to u8.8 format. |