DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
Flash read may be performed by the main application in Standby mode. The entire flash may be read, or a flash block may be selected to be read. The main application determines whether each flash block is stored in flash or EEPROM, if it is in use. Therefore the procedure is identical for reading EEPROM.
The following commands are used to read flash data:
Figure 5-18 demonstrates the flash programming steps.
The read command handler flow described in Section 3.5.4 should be used for each of these read command transactions to ensure that the read data is available prior to a retrieval attempt.