DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
If the source was initially in-range, a failure will trigger the display of an alternate internal video source. This can be configured as any test pattern or splash image stored in flash. If the source is initially out-of-range during configuration or during a transition to display, no image will be displayed.
Table 6-5 describes various source scenarios and the action that will be taken.
CONFIGURATION | EVENT | ACTION |
---|---|---|
Source valid | Standby to Display transition | Display external source |
Source invalid | Standby to Display transition | Stay in standby
Log Error |
Source valid | Source select command | Display external source |
Source invalid | Source select command | Illumination disabled
Log error |
Source valid | Source valid to invalid | Display alternate image
Log error |
Source invalid | Source invalid to valid | Display external source IF auto-recover |