DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to set TPS99000-Q1 RGB DAC levels. There are multiple groups of RGB DAC levels that may be used within a sequence. A group is specified and then the three DAC levels within that group are provided. Note that sequences may use a minimum of one group. Setting the value of unused group DAC levels will have no effect on the displayed image. Typically group 0 is used by all sequences.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 1:0 | Group 0 - 3. |
3:2 | 11:0 | Red Group DAC Level 12-bit, 0 - 4095. |
5:4 | 11:0 | Green Group DAC Level 12-bit, 0 - 4095. |
7:6 | 11:0 | Blue Group DAC Level 12-bit, 0 - 4095. |