DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to specify the System Mode index. The available System Modes are specified in the flash header file that is included along with the flash data. This command is not applied until a source change is requested. Section 10.2 provides an overview of system modes.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | System Mode Index First index = 0 |