DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to read the flash structure version of the current flash build. Each main application expects a certain flash structure version. Flash programming will fail if the flash structure version of the incoming data does not match the version that the main application expects. Note that this is different than data-dependent versioning. Data-dependent versioning is performed with flash block CRCs.
Command Parameters
No command parameters.
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
2:1 | 15:0 | Flash Structure Version - Patch LSByte = Byte 1 |
3 | 7:0 | Flash Structure Version - Minor |
4 | 7:0 | Flash Structure Version - Major |